This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53219A: TPS53219A

Part Number: TPS53219A


TPS53219A的DS标称输入电压范围为3V~28V,然后使用webanch设计工具,输入电压范围却被限制在了最大24V,而我实际使用芯片发现当输入大于24V确实会出现一些问题,请问这是怎么回事?

  • Hi

        是Webench在先仿真参数设置错误, 正常应该是28V. 

        你可以用8~24V做仿真,但是实际28V输入也是没有问题的。   (直接套用这个电路来用,将webench上24V当作28V)

        或者你按照datasheet 中的计算来确认芯片周边参数也是可以的,只是没有Webench仿真方便。