This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD17573Q5B: 推動相同電流MOSFET(High Side)溫度會隨著架構不同而不同,怎麼設計以降低MOSFET溫度

Part Number: CSD17573Q5B

如要搭配下方Gate Driver, Rg(R50, R52), Rgs(R1, R319), Cboot(C27), Rnode(R51)該怎麼設計以降低MOSFET溫度?

理論上這顆MOSFETRdsOn已經夠小, 但我們實際操作在下方架構8A就有過溫問題, 之前用其他的Buck Converter IC搭配這顆MOSFET可以到達20A(Converter操作頻率約200KHz)

 

  • 已有使用直流確認該MOSFET的8A導通溫度是正常(40度以下), 因此已排除是RdsOn過高和包裝熱阻過大的問題
  • 目前傾向往切換損失的方向驗證, 是否是該Driver推動電流或是斜率不匹配造成, 是否有建議修改的方向?  Rg(R50, R52), Rgs(R1, R319), Cboot(C27), Rnode(R51)?
  • 請問TI是否有推薦能推動csd17573q5b的Half bridge Driver IC以及建議線路供我們參考?

Driver IC: Infineon-2ED2101S06F

Driver Voltage: 12V

Driver Input: 80KHz PWM (Gen by MCU)

Driver Output: Half Bridge, 2 MOSFETs (TI csd17573q5b)

Power Input Voltage: 20V

Power Ouput Voltage: 12.8V

Schematic: below (Buck Converter, Current flows from right to left)