This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GU10隔离调光方案的问题



 GU10隔离调光方案由于空间的限制,所以要求很小的pcb尺寸,另外一个重要的问题是对调光器的兼容以及调光的稳定性

原文链接http://www.deyisupport.com/question_answer/analog/led_lighting/f/76/t/29111.aspx

TI的回答了此问题

PMP4339设计原理上来看,由于追求性能的稳定以及调光方案本身的因素该调光方案所使用的元器件还是比较多的,而且还带高PF,如此小的pcb空间是否会为生产带来麻烦,但从DEMO板来看觉得还是不成问题的, 个人觉得调光器兼容性才是一个最大的问题,由于调光电源的兴起,调光器的品牌也越来越多,在调光比较暗的时候可能会有一定的闪烁,不知道该方案的兼容性是否在90%以上,这些在帖子中都没有详细的描述,另外还有工作电压范围,在85V~150V的工作电压用PMP4339如何设计,能否设计出85V~265V全电压工作的调光方案,尺寸问题是解决了,但批量生产的一致性如何,这些还期待TI的FAE解答,谢谢