This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: 应该如何设置寄存器才能满足需要的功能?

Part Number: BQ25703A


这是测试板的原理图:

电池是单个锂电池:4.2V满电。

电池充电电流:1A.

VBUS是USB输入的5V电压。

一、需要的功能:

1、没有电池的情况下:

     连接USB,VBUS此时5V,我需要VSYS+得到5V的电压输出。

2、有电池的情况下:

      1):连接USB,此时需要给电池充电,并且VSYS+依旧有5V输出。

     2):断开USB,VSYS+依旧有5V输出。

3、在所有模式下均能读到充电状态、电池的实际电压。

二、测试板异常现象:

1、连接USB时,I2C可以和BQ25703A通信。断开USB时,无法与BQ25703A通信。

2、连接USB,BQ25703A没有给电池充电。

根据以上,请求帮助,MCU端需要给哪些寄存器设置什么值?谢谢大家!