This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: bq76952

Part Number: BQ76952

BQ76952在什么几种条件下能进入预放电模式?在几种条件下可以退出预放电模式?技术手册上讲的不是太清楚

  • 您好,

    There are two ways to enable the pre-discharge FET initially. Either through timeout or through a voltage condition set by Settings:FET:Predischarge Stop Delta.

    If using timeout, the PDSG FET will be enabled initially until the timeout time occurs, where the DSG FET gets activated. With a voltage condition the PDSG FET will be enabled initially until the Predischarge Stop Delta condition is met, then it will transition to activating the DSG FET.

    If the DSG FET is already active, the PDSG won't be activated unless the DSG FET is turned off and on again (This could be done through commands).

    See Section 5.2.3.2.2 PREDISCHARGE Mode of the TRM for a description and functioning of the PDSG function.

  • 感谢您的回答,您说的设置的超时和电压应该是退出预放电模式切换到主放电管开的条件吧,不是进入预放电模式的条件吧,在初始状态,在电流为0或者在sleep模式下,主放电管是开启状态,无法实现自动关闭,只能通过命令实现DSG FET关闭,此时通过检测到负载接入,先开启预放管,等到达到设置的超时或电压条件达到自动退出预放模式,开启主放电管,不知道我的理解的逻辑是否正确?

  • 您好,是的,你可以实际验证一下。