Other Parts Discussed in Thread: TPS5430
你好,我想请教下以下几个问题:
1、TPS5450的datasheet上推荐电路,电感值算出来是10.4μH,推荐为15μH。但是根据手册给出的电感计算公式
,输入31V.输出5V.电流5A,系数为0.2,开关频率为500K,算出来跟芯片手册上并不一样。
2、之前测试时候,24V上电能正常输出5V,但是第二次上电后芯片就烧了,电路与datasheet上的应用电路完全一样,请问下有哪些可能性造成芯片被烧?
3、TPS5450与TPS5430的datasheet给出的纹波电压公式不同,以哪个为准?
(TPS5450)