Other Parts Discussed in Thread: UCC28810, UCC28811, TPS92001
我目前在做几个60W以下的单级PFC,LED电源。
全电压输入,PF>0.95,输入谐波电流小于20%。
效率83%以上,全电压输入。
最好能有输出短路保护功能的。
请帮推荐一下你们有哪些IC可以选用呢?另UCC28811各UCC28810有哪些不同?另UCC2811的PDF资料能否给份,因一直没有找到。非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用UCC28810/UCC28811设计就可以,见TI官网: www.ti.com.cn/.../ucc28810
两者参数差不多,公用同一个datasheet, 没有独立出来,差异可以见datasheet 第二页描述和第四页参数表。
除了你提到的IC外还可以考虑TPS92001/2等,同时你也可以通过 <2011电源管理选型指南> 系统地了解LED照明的解决方案