This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 初步使用过程遇到的一些问题

Part Number: BQ34Z100-G1


TI,

你好!

目前我们的系统在使用BQ34Z100-G1测量铅酸电池组电量,铅酸电池4节,12V13AH,ChemID设为0809,自学习已经成功,UpdateStatus=0x06,但在初步使用过程中发现一些问题:

1、自学习成功后,系统充电SOC达到100%,然后系统多次断电后重新上电,SOC电量分别显示为96%、90%、88%、87%~75%,每次重启后SOC逐渐变小,为什么?有什么根本解决措施?
2、系统充满电后电量显示100%,系统断电重启后,开机时显示电量只有80%~90%左右,此时如果充电,SOC会短时间内从80%左右突变到100%,为什么?有什么根本解决措施?
3、自学习成功后,系统使用过程中断电重启,发现FullChargeCapacity比原自学习时容量变小,为什么?有什么根本解决措施?
4、自学习成功后,IT_ENABLE、Reset、SEALED然后操作?次序有什么要求?生产设置步骤有哪些?请说明一下。

以下是gg文件和log文件,是否还存在错误?ChemID是否合适或更新?请给予我们协助与指导,非常感谢!!

GenesisBat-20230508-0856_toTI.gg.csv2023-0506-0939.log2023-0511-0931.log