This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: 充满后FC=1,静置很长时间寄存器都不跳变

Part Number: BQ34Z100


奇怪的是明明已经断开充电器,remaining capacity 和 full charge capacity居然还在上涨

充满后REST寄存器没有跳变,这是什么原因?

另外,我买的是3.2V磷酸铁锂电池,但是此电池满充时达3.8V,一旦停止充电,会在一小时内掉电至3..3V,这样的电池是否无法进行阻抗跟踪学习?

  • 您好,从您的画面上看还有电流,所以RM和FCC会变。请确认电流是否校正。

    铁锂电池因为平坦区特别宽,阻抗跟踪算法的性能可能不是很理想的。

  • 谢谢Star Xu您的耐心回复,电流校正这个其实之前也提问过您, 您给出的建议是用1A的电流进行放电校正,不过我现在手头上没有1A的负载,所以也没有好办法。另外我发现在我校正电流时可以填写大于等于100mA的数值,小于100mA的电流就会出现上图中的错误,这可能是什么原因造成的呢?