This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: 电池未放到Cell Terminate Voltage,SOC和RM突变为0

Part Number: BQ34Z100-G1


你好,

最近我在使用新的LFP电池(已修改ID),配置完Golden Image后发现几个问题

#1_我在放电过程中RM, SOC, 突然变为0, FCC值也骤降, 我设置的Cell Terminate Voltage为2200mV

#2_我在放电结束后PassedChg为6630mAh,CC Threshold设置值为6200mAh,但是我的Cycle Count和MAXERROR并未增加

请问能否解答我的疑惑

真诚感谢