This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2662: TPS26625 FLT 电流是 leakage current还是sink current

Part Number: TPS2662


问题一
TPS26625的SPEC写 FLT active LOW 时 , input leakage current 最小是-100nA
最大是100nA , 当FLT active LOW 时内部的MOS 是 ON 应该不会有leakage current
请问input leakage current 使指什么电流?
FLT 应该只有 Sink 电流 , 所以input leakage current就是sink 电流吗?

问题二
input leakage current 最小是-100nA 最大是100nA
为何会有-100nA , 正负符号不是代表sink跟source
FLT 只有sink 所以应该只有正符号

问题三
TPS26625的SPEC写sink current 10mA , 表示FLT脚位最大的sink电流是10mA
所以计算FLT电阻最大可用10mA计算,还是要用input leakage current 计算呢?
sink current等于leakage current 吗