This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求电源芯片



12V的输入,输入电流大约为10A左右,要求输出端最好是二路输出端,其中一路的输出电压为8V to 15V,输出电流不超过3A;另外一路输出可以为3.3V,电流不足1A左右就好。芯片最好是12--14年出的。