This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照datasheet第八页的公式:
按照最严的规格IoutMax=5A 而lCL=5.75A, 算的Fsw=250kHz
也就是说当频率较高出250kHz时,纹波电流会更加的小, 可以做到最大输出5A.
电感的计算参照datasheet第十三页:
采用Fsw=500kHz, 最大输出5A, L=(20-15)*15/(0.3*5*500k*20)=5uH, 所以你选择4.7uH也可以。
但是此时电感峰值电流刚好是5A +5*0.3/2=5.75A, 意味着你的频率需要大于500kHz 才能合适。
HI
比较好的选择是将电感的裕度稍微留大一点,例如选择7A以上。
电感选用时要考虑过载测试时,电感不能饱和,设计余量要留足。