有一个+5v的输入,有没有什么典型的电路能够输出+/- 10v的输出电压,且为100ma的输出电流呢?我看到一个tps61093可以输出+/- 10v,但是输入为3.3v了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有一个+5v的输入,有没有什么典型的电路能够输出+/- 10v的输出电压,且为100ma的输出电流呢?我看到一个tps61093可以输出+/- 10v,但是输入为3.3v了
HI
TPS61093是1.6~6V输入,所以即便是5V输入没有的。可以直接套用这个电路,只要注意功率电感饱和电流足够即可。