1.看block 器内部调整管是Pmos,想请问该管子在降压时是工作在饱和区吗?
2.想详细了解下,当输入电压变化和输出电流变化时,内部调整管是是如何工作,是输出电压稳定的?
3.对于LDO,不论是PMOS LDO,还是NMOS LDO,其Vdrop电压是否等于Vds电压,例如TPS799在输入,输出3.3V,200mA电流时,Vdrop是否等于160mV,内部MOS管Vds是否也等于160MV,当输出变化时,100mA时,Vdroph和Vds应该是多少呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.看block 器内部调整管是Pmos,想请问该管子在降压时是工作在饱和区吗?
2.想详细了解下,当输入电压变化和输出电流变化时,内部调整管是是如何工作,是输出电压稳定的?
3.对于LDO,不论是PMOS LDO,还是NMOS LDO,其Vdrop电压是否等于Vds电压,例如TPS799在输入,输出3.3V,200mA电流时,Vdrop是否等于160mV,内部MOS管Vds是否也等于160MV,当输出变化时,100mA时,Vdroph和Vds应该是多少呢?
Hi
1. 工作在线性区。
2. 通过反馈调整。
3. Vdrop是MOS的导通压降。
HI
LDO又称线性电源转换器,即内部MOS工作在线性区,这样可以通过反馈调整输出。
VDS实际上就是输入输出的压差, 而Vdrop则是LDO维持正常输出的最大压差。如你举例4V输入3V输出,VDS就是1V, VdorpMAX是80mV, 那么最低输入就是3.08V(考虑到纹波之类,建议适当略高一些)。