Other Parts Discussed in Thread: USB2ANY
你好:问题如下:
环境配置:bq79616evm-021 ,usb2any,GUI. 16节3.7V电池,跳线J14 和J16均短接。并对cell16s和pwr信号进行了短接,充电工具:71.4V,2A,充电器。
问题1:当打开充电器时,约10秒后,通讯中断,为什么?
问题2:第16节电池正极连接到cell16信号,如果不对cell16s和pwr信号进行短接,不能对第16节电池测量,对这两个信号的短接是否正确?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:问题如下:
环境配置:bq79616evm-021 ,usb2any,GUI. 16节3.7V电池,跳线J14 和J16均短接。并对cell16s和pwr信号进行了短接,充电工具:71.4V,2A,充电器。
问题1:当打开充电器时,约10秒后,通讯中断,为什么?
问题2:第16节电池正极连接到cell16信号,如果不对cell16s和pwr信号进行短接,不能对第16节电池测量,对这两个信号的短接是否正确?

您好,请参考下面内容
Please remove the J14 and J16 jumpers. Additionally, the power supply positive terminal must be connected to the "PWR" testpoint, and the power supply negative terminal must be connected to the "Cell0" testpoint since you are not using the resistor ladder cell simulator.
If this does not help with the issue, please send me a detailed diagram or picture of the setup so I can better diagnose the issue.
您好:
因为pwr和cell16是同一信号,所以电池组的正极通过J15的21脚接入cell16,再接入到pwr,似乎并没有问题。
去掉J14和J16,任然会在充电时通信断掉。
去掉J16会导致另一个问题:cell1的测量不准确,插上J16,cell1测量准确。
以下是我的测试条件及结果,劳驾解答:
1,环境条件: 第16节电池正极通过J15的21脚接到cell16,第1节电池负极通过J15的3脚接入cell0,把pwr和cell16s短接,充电正极节pwr,充电负极接cell0s,插上J14和J16,无负载
测试结果:充电几秒后,通讯中断。
2,环境条件: 第16节电池正极通过J15的21脚接到cell16,第1节电池负极通过J15接入cell0,把pwr和cell16s短接,充电正极节pwr,充电负极接cell0s,去掉J14和J16,无负载
测试结果:充电几秒后,通讯中断。cell1的测量不准确,电压会高约0.3V左右
3,环境条件: 第16节电池正极通过J15的21脚接到cell16,第1节电池负极通过J15接入cell0,把pwr和cell16s短接,去掉J14和J16,不充电,无负载
测试结果:cell1的测量不准确,电压会高约0.3V左右
4,环境条件: 第16节电池正极通过J15的21脚接到cell16,第1节电池负极通过J15接入cell0,把pwr和cell16s短接,去掉J14,插上J16,不充电,无负载
测试结果:16节电池测量全部正确
5,环境条件: 第16节电池正极通过J15的21脚接到cell16,第1节电池负极通过J15接入cell0,把pwr和cell16s短接,充电正极节pwr,充电负极接GND,去掉J14和J16,无负载
测试结果:充电几秒后,通讯中断。
您好,感谢您的回复,正在询问更了解这款芯片的TI工程师,稍后回复。
如果怀疑是评估板的问题,请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。
您好 ,看您分享的图片,看起来您的连接如下

With this setup, the customer does not have a connection for CELL0S or CELL16S. This is why removing the J14 shunt causes CELL1 voltage errors, and had problems with CELL16 and PWR, causing them to short the 2 points together.
Please address the J15 header connection issues, populating CELL0S and CELL16S. You can then remove J14 and J16, as well as desoldering the wire from the Cell16 test point to the PWR test point.
Additionally, the negative terminal of the charger should be connected to the CELL0 TP, not GND. Please also look at the BQ79616EVM User Guide for the EVM schematic to confirm any connectivity issues: BQ79616-Q1, BQ75614-Q1, BQ79656-Q1 Evaluation Module User's Guide (Rev. B).
您好,同样的测试有两块板子有异常应该是板子的问题。请参考下面的内容帮助您确认如果是板子的问题是否能帮您更换板子。
请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。