This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
the BQ40Z50-R2 is a SMBus charger and potentially can control the BQ25792 which is an I2C charger. Please see the file <www.ti.com/.../sloa132.pdf control an I2C device with an SMBus host. However, even if this works, you cannot have two primaries on the line.
The best solution I have for you is to use a MCU. The gauge would talk via SMBus to the MCU, which would then in turn talk to the TPS25750. The TPS25750 would pass through the commands to the BQ25792. This will ensure no bus collisions.
详细请参考下面帖子的内容:
Hi Star,
thanks for your information,
i also viewed the topic of the link, it seem can use same I2C bus line for TPS
25750 and BQ40Z50_R2, battery charger be controlled by TPS25750's I2C master . there is no any collisions on I2C and SMB bus, right? the connection figure is as follow
您好,是的,上面推荐的解决方案是使用 MCU。BQ40Z50通过 SMBus 与 MCU 对话,然后 MCU 与 TPS25750 对话。 TPS25750 会将命令传递给 BQ25792。这将确保没有总线冲突。