This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询是否有恒流源,输入12V-24V,输出65Z左右的升压恒流芯片



你好,贵司是否有升压恒流芯片,启动速度可以控制在10ms以内的。

但是需要多个芯片拼接使用?

目前用TPS92961实现了,启动速度OK,但是多个板子无法做到一致性。

我们是采用TPS92961实现对三路MOS驱动输出并联,目前测试发现,最大板子与板子之间最大功率差距是400mA。这个一致性不行,所以需要寻找如下芯片:

1.升压

2.启动速度可以通过外部电容设置,目前想做到10ms以内

3.可以通过信号同步所有拼接的板子,做到亮度基本一致(就是输出功率一致性高,最大差异大概20mA以内).

请尽快帮忙支持下。