Lm5114B用在高频逆变器做Mos管的驱动级时,工作频率为13.56Mhz,示波器看到的Lm5114B的输出波形会失真,甚至在板子上看到的方波发生器的输出也会失真,但单独直接测方波发生器的输出是正常的,您知道这是什么原因吗?附图是我采用的电路,是Lm5114连接不对吗?非常感谢您的回答!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Lm5114B用在高频逆变器做Mos管的驱动级时,工作频率为13.56Mhz,示波器看到的Lm5114B的输出波形会失真,甚至在板子上看到的方波发生器的输出也会失真,但单独直接测方波发生器的输出是正常的,您知道这是什么原因吗?附图是我采用的电路,是Lm5114连接不对吗?非常感谢您的回答!
HI
你的意思是单独用信号发生器测试LM5114, 并且驱动输出不带MOS,是可以正常有方波输出的? 但带上MOS就会在高频率下异常? 有没有降低频率后会正常?
这类芯片主要麻烦在于datasheet并未明确最高频率,而常见的应用都是低于1MHz的。
Hi
我担心的是芯片不能用于这样的高频应用,建议你将驱动电阻拿掉,另外确认一下供电Vdd是否稳定?
Hi
Vdd供电使用的是稳压源,芯片的out到栅极有一段距离,在去掉驱动电阻后,稳压源输出为5V/0.03A,禅师这种情况的原因是不是没有保证输出到栅极尽可能短?