我在使用LM3410时,当我接入电池的时(没有接LED灯板),LM3410的输出电压为22.5V(正常工作时的电压为7V到9V之间),此时当我接入LED灯板时,会击穿R60/R50/M50/M4其中的一个,或者是多个,能帮忙分析一下是什么原因导致的吗?
1、上电时为什么LM3410在没有LED灯板(负载)情况下的输出电压为22.5V,只要不去调节灯光,这个电压一直存在
2.正常供电时,接入灯板LM3410和R60为什么会击穿2023-02-17_SkinnyDuo_CTRL_MFG 2023-02-17_SkinnyDuo_LED_MFG.zip
3.期待各位大神帮忙分析一下,很着急