This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088: LM5088输出负电压:-62V,芯片发烫

Part Number: LM5088


LM5088输出负电压:-62V,12V输入。输出电压正常,但是LM5088芯片在短时内迅速升温至80摄氏度,这是2层板的现象;如果改成4层板,中间两层是电源平面,LM5088也是迅速升温,不过温度只有50摄氏度。请问导致LM5088芯片升温的主要原因是不是内部的regulator输入电压过高导致?原理图如下:

  • Hi

        输入输出压差74V,接近芯片极限耐压75V,  所以首先需要确认输入,输出是否有过充或者不稳定之类?

        其次从规格上看,峰值电流会很大,你还要需要确认功率电感饱和电流足够,同时选择Qg尽量小的MOS.

        最后,如你所说VCC消耗较大是需要注意的,你可以适当选择较小的频率(300kHz左右), 芯片底部Powerpad需要充分和GND焊接,并且充分扩展GND面积用于散热。