Other Parts Discussed in Thread: LM5010
输入电源 57.4V,
输出12.5v,加载后电流195mA
原理图
LAYOUT图
目前测试已烧毁 14PCS,约
13-6 1PCS
13-6-2 5PCS
13-5 1PCS
13-2 3PCS
12-3 5PCS
可否询问一下,这样的设计是否那里有问题呢?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
输入的2.4mH电感建议去掉,原因是在前面等效增加了一个升压电路,在瞬态启动时,电感电流电流时,电感上可能因为感值这么大的电感而产生一个较高电压,而你本身的输入电压已经达到57V了,所以在后端电容无法稳压而造成一个较高的震荡,而直接烧13脚,13脚过压造成的芯片烧掉,现象是各种各样的。
这一现象你可以用示波器测试板子的启动电压得到证实。 建议你将电感改小,而增加输入电容的容值,电感前面靠近输入connector也可以增加一个电容100uF.
Hi
US1G是超快恢复的TVS管,在这类电路中用到的应该是超快恢复的整流管,两种应该是有差别的,不应该会用到前者。