This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24725A: 给单节锂电池充电,接入负载后配置寄存器充电电流影响实给电池充电是什么原因?是因为充电器的输出限制吗?

Part Number: BQ24725A


现象:

1、ILIM管脚的电阻配比是316kΩ/100kΩ

2、寄存器配置的充电电流为4A,充电电压配置为4.2V,可能是由于接入的充电器输出限制,实际充电电流为3A;

3、当我接上负载后就不会给电池充电了,但当把寄存器配置的充电电流改为小于等于3.2A后可以给电池充电;

4、并且当我充电电流配置好后,实际充电电流总会比配置的小是什么原因?例:配置充电电流3A,实际充电电流只有2.3A。