Other Parts Discussed in Thread: TPS43060, LM5122
工程师你好。
1.请问关于TPS40210,GDRV引脚的驱动电平是多少?
2.对于这一类外接MOS的驱动器来说,是不是可以理解成:只要MOS电流可以承受,那么整个BOOST电路的输出电流就可以无限增大?
3.针对此类驱动器,外置NMOS一般该如何选型?参考驱动器的哪些参数呢?
感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
1. 驱动电压来源于Vbp,VDD高于8V(以上)时, Vbp电压输出8V左右(略低),即驱动输出电压。如果VDD较低(低于8V), Vb作为LDO输出也会相应偏低。
2. TPS40210输出能力并不强或者说驱动能力不强,一般电流不建议太大(不建议超过4A)
3. N-MOS选择Qg, Rdson尽量小的即可。
HI
1. 驱动电流比较小, 并非驱动电压。
2. 你可以借助webench在线仿真选型,例如TPS43060, LM5122之类,相对功率可以做得比较大。
Hi
频率越高,芯片消耗越大。
你需要理解MOS是电压驱动型,芯片驱动电流将MOS G充电到驱动电压。