This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54531: 低概率输出电压降低

Part Number: TPS54531


问题:

型号 TPS54531,按参考电路设计,输入是固定的 24 V ,输出是 7 V,EN 引脚电压为 5.5 V, 负载电流在 100 ~ 200 mA 之间,有千分之一概率出现输出电压下降至 3~4 V 甚至 1 V 的情况,产品生产过程和销售使用后均有出现,更换芯片后电路正常,请问可能的失效原因及规避措施是什么 ?