Part Number: LM5022
标题这句话怎么理解?
目前如果这边的VIN电压最小只有3V,请问这个地方有没有什么方法启动芯片工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照datasheet 第一页描述: VIN 范围:6V 至 60V(启动后,最低可以在 3V 下工作)
这边的意思是说,VIN提供3V电压也是能正常工作。这里有提到启动后是指什么?
Hi
就是芯片启动之初输入电压需要大于6V, 在工作中输入电压再下降,低至3V仍可以正常工作。