This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360B-Q1: 技术咨询

Part Number: TPS54360B-Q1


你好,

     产品选型DC/DC要求如下:

       1、输入电压:6.5V ~ 36VDC

       2、输出电压:5.8V/500mA

       3、工作环境:-40 ~ 125℃

       4、产品应用:汽车级电流传感器

       5、EMI/EMS III级

       初步选型为TI DC/DC TPS54360BQDDRQ1,根据TI网站提供的硬件设计配置方案,进行设计,现有以下问题,需确认:

      (1)芯片选型是否合理,帮评估;

      (2)加入EMI 滤波,线路阻抗,RZ、LZ,是否合理?

(3)最终的推荐外围参数如下,帮忙检测,是否合理?

(4)由于PCB空间的原因 电感L1,选用MWSA0603-220MT ,DCR:200mΩ,影响有多大?