This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088: tps61088升12V,输入电压大于10V时会烧毁。

Part Number: TPS61088


使用tps61088升压至12.4V使用。输出电流峰值为3A左右,稳定时不到1A。当输入电压低于10V时,该升压模块可以正常使用,不会烧毁。当输入电压大于10V时,12.4V输出侧开关闭合,芯片会直接着火烧毁,着火处为tps61088的SW引脚处。希望各位工程师能找找问题,或者推荐同场合其他可替代使用的芯片。原理图,pcb如图。