This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65911 VDDCTRL高端电压的问题

Other Parts Discussed in Thread: TPS65911, TMS320DM8148

TPS65911     VDDCTRL参考电路高端电压为12V,由于我们系统为24V系统,系统中除了此处要求12V外,没有其他需要12V的地方。

我想问以下几个方面:

(此处调节电压输出电压为1.2V,使用的是TMS320DM8148开发系统)

1、用户手册中第83页,寄存器VDDCRTL_OP_REG设置说明:VOUT=(SEL[6:0]*12.5mV+0.5625V),此处0.5625V是固定设置吗?还是与外部高端电压12V有关?

2、由第一个问题,外部MOSFET高端电压12V能否改成5V供电,修改后寄存器的配置是否需要修改。