This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z561: 电池在静置时,电量计剩余容量缓慢上升原因

Part Number: BQ27Z561


Dear all,

电量计BQ27Z561运用中碰到一点问题,请帮我分析下,非常感谢!

我们有一个项目使用了两块电池,两块电池放在一起,环境条件相同,两块电池都使用了BQ27Z561电量计,电池A容量1210mAh, 电池B容量2750mAh,测试数据通过系统打出的LOG,因为两块电池是并联的,当系统停止充电后,两块电池之间会有小电流进行互相充电。

问题:
1. 当互充结束后,电流已经基本上是0mA了,但是电池B的剩余容量一直在上升,涨了约120mAh;
2. 互充结束后,电池A的剩余容量则没有发生变化;
请问下这是什么问题?在相同的环境下为什么两块电池的现象会不一致?
详细LOG请查看附件,记录周期约每1.5秒一次。