This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: OTG模式输出的时候可不可以插适配器充电

Part Number: BQ25703A


1、BQ25703A芯片在OTG模式输出电压的时候,可以直连适配器进行输入吗?OTG输出电压12V,适配器输出5V

2、如果不能,那么芯片OTG输出模式的时候,能不能通过读寄存器来确认有没有负载?谢谢

  • 您好,USB On-The-Go (OTG) 是通过USB充电。

    负载检测请看数据手册表 15. ProchotOption1 Register (I2C address = 39h) Field Descriptions

    IDCHG Threshold:Trigger when the discharge current is above the threshold