This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在进行电池学习的过程中,将电池放电到截至电压以后,由于有这些led灯,电压一直往下掉,这影响到了实验数据。无奈将J6上的跳线给拔了,这样做是否会影响实验结果?
您好,If you do not use the LEDs or ALERT function, then the J2 and J5 jumper blocks are the only ones that need to be configured. You would set the shunts in the >5V positions on J5 and the 32V position on J2. You do connect BAT+ and BAT- to the battery and BAT+ and PACK- to the load or charger. The computer should recognize the EV2300 after you connect the USB cable. You could try power cycling the computer.