This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP877451Q1EVM: cs脚应用咨询

Part Number: LP877451Q1EVM


Hi TI的专家们,

我在使用877451的时候遇到一个问题,关于PIN4(CS_SPI/WD_DIS),我们采用了2.2K的下拉,使得刚上电时默认关闭877451的看门狗(不关看门狗,我们无法通过串口给2944烧录程序),

我们最近贴了两批次同样的PCBA,PCB和物料均是同一批次,但是两个批次,未烧程序前,上电测量CS状态,发现CS状态不一样,导致有个批次的PCBA上877451的看门狗无法关掉,一直在周期性输出reset,周期大概为4.94s,如图中绿色方框里面的

我测量了两个批次的87745的CS状态,能关掉看门狗的PCBA上的CS测试状态如下,会先有一个小脉冲(绿框内),然后会一直保持一个0.11V左右的低电平,

CS异常的PCBA测试结果如下图,同样会先有一个小脉冲(绿框内),然后会上升到3.3V,我分别试了更改CS下拉电阻阻值(2.2K/1K/499/200/100),这个PCBA的CS引脚的上电波形不会变,

我看规格书上CS内部是有一个1M的上拉和2.85M的下拉,理论上外接2.2K左右的下拉,应该能把CS的电压拉到0.1V以下,关闭看门狗,

请帮忙看下为什么我这两个批次的板子会出现不同状态,CS的下拉阻值该如何选择?

谢谢。