我在用户手册的9.2章节有看到通信子系统的描述,想了解下各个尾缀如BQ7695202在初始上电时时钟默认频率是多少?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The I2C serial communications interface in the BQ76952 device acts as a responder device and supports rates up to 400 kHz with an optional CRC check. If the OTP is not programmed, the BQ76952 device will initially power up by default in 400 kHz I2C mode,