您好!我现在用BQ40Z80配置6节锂电池,我在进行放电测试时,将Term Voltage电压设置为18600mV,但是我的电池放电到这个电压时,并没有停止放电,请问一下是什么原因?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请参考文档
3.6 Term Voltage
Also called Terminate Voltage, this is essentially the empty pack voltage where the gauge should ensure
0% state of charge is reported. For learning cycle purposes, this should be set to the minimum voltage of
the battery as specified in the manufacturer’s data sheet. After the learning cycle is completed, this value
can be adjusted upwards if there is a need for the gauge to report 0% at a higher voltage. If the cell is
rated to operate from 3 V to 4.2 V and if the application is a 5s application, the term voltage should be set
to 3 V x 5 cells = 15000 mV. This setting is in the Gas Gauging, IT Cfg section of Data Memory.
Note that in normal operation the gauge may report 0% at a voltage higher than Term Voltage because it
learns the voltage spikes seen by your system. The adds the average of those spikes to Term Voltage in
order to predict empty at an earlier voltage so that a sudden spike does not cause a drop to 0%. These
learned average spikes are kept in RAM but occasionally updated in the dataflash parameter Delta
Voltage. Additionally, if Reserve Cap-mAh and Reserve Cap-cWh are not zero then the gauge further
buffers the voltage at which 0% is reported in order to ensure that the reserve capacity is still available for
shutdown before Term Voltage+Delta Voltage is actually reached.