This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LT1054: 关于DCDC芯片输出电流大小的问题

Part Number: LT1054

我用的DCDC芯片是LT1054,它的最大输出电流可以达到100mA,但是它的输出电流一定可以达到100mA吗?这个输出电流和什么有关呢?我在datasheet没有找到相关数据和表格。只知道可以通过调节R1和R2的阻值从而达到输出电压的不同,但是输出电流如何调节呢?

此外,如果DCDC芯片的输出电流由它的负载决定,因为DCDC芯片后级电路是放大电路,而仪表放大器芯片的输入阻抗很大,为GΩ级别的,也就是负载的阻值很大,那DCDC端输出电流不就会很小很小吗?那这样可以驱动后级放大电路吗?