我使用了TPS3813K33型号的窗口看门狗,我的程序是30ms的周期在运行,使用看门狗的场景为在每个30ms的周期内,设置程序运行到24ms-28ms的窗口内进行喂狗操作,窗口外的时间喂狗就会被复位。
现在遇到的问题为:我通过WDT引脚设置上边界时间的时候,当使用155pF的电容,Tw=68ms(这已经是最小的状态了),好像无法设置到30ms以内。
以上是不是说明这个看门狗芯片无法实现我的需求?或者说是我对这个看门狗的使用方法理解有误?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在datasheet 第7页有规格表和计算公式。如果要更端的Tout, 使用更小的Cwdt看看,例如15pF.