This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542EVM: FAC和FCC降低很快,导致SOH降低

Part Number: BQ27542EVM

在使用电量计BQ27542-G1的电量计时候,确认FCC、FAC的容量掉得很快,做了几个循环后,FCC就从2700mAh降到了2000mAh;
在使用的过程中,电池包不会进行满充和满放;但是FCC的降低影响到SOH跟着下降;
请教下可能发生的原因是什么?
以下是测试的数据和gg.file LI-320 data and gg file.zip
充电截止:恒流恒压充电至FC置位;
放电截止:以剩余容量(RC)的8%停止放电;

测试条件:
周一到周四:
1、电池包正常充电至FC置1后;
2、以50mA~70mA 的电流放电约15h(约30%的电量),静置约6h;
3、循环①和②步四次;
周五至周一
4、电池包正常充电至FC置1后后;
5、以约9mA放电至FC清0,然后继续充电至FC置1
6、循环④和⑤步至周一;
7、持续循环①和⑥