This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65296: 8PCS LPDDR4供电方案确认

Part Number: TPS65296


我们计划使用8pcs MT53E2G32D4   LPDDR4,根据数据手册计算得到8pcs DDR所需最大电流数据如下

VDD1=1.8V,1.088A

VDD2=1.1V, 7.536A

VDDQ=0.6V,1.28A

TPS65296芯片数据手册给出的供电能力如下

VDD1=1.8V,1A

VDD2=1.1V, 8A

VDDQ=0.6V,1.5A

想确认TPS65296能否支持8pcs MT53E2G32D4 LPDDR4的供电