Part Number: BQ24295
TI的工程师你们好!
我想运用BQ24295这个芯片设计一个单节锂电池充放电,且放电电压可调(5v-20v),电流不做要求。主控芯片为stm32f103c8t6,通过I2c与其通信,实现电量实时显示和电量警报功能。
想请问你们有没有适合参考的原理图呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
BQ24295是一款单节电池充电器。 当电池放电时,最大电压将是电池的电压(4.2V 范围内)。 此器件能够运行在升压模式中,但是最大输出电压为5.5V。 允许的最大 VBUS 电压为6.2V,如数据表第1页所列。
BQ24295EVM 设计原理图可在 TI.com 上的 EVM user guide中找到: