This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: PWM控制电流输出温度高,短路保护时ST引脚输出异常

Part Number: TPS1H100-Q1


1.用TPS1H100AQPWPRQ1来进行PWM控制电流输出时,工作时温度非常高,有100℃左右,一开始频率设置在2000Hz,认为是频率达到了上限,后来把频率改成1000Hz后,温度还是很高,实际项目至少也的1000Hz,输出的电流最大1000mA

2.做短路保护时,将VOUT短接GND时,会有吱吱声,诊断PIN的ST引脚只有0.4V的压降?