This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG3422R030: Design problem of three-phase bridge based on LMG3422

Part Number: LMG3422R030


The three-phase bridge circuit is designed with LMG3422, which is used to drive the three-phase brushless DC motor,Three-phase UVW is connected with three fuse tubes in series. When the fuse tube has 10A replaced with 1A, the fuse tube will be burned. At the same time, alarm will appear on the W upper tube, W lower tube and U lower tube in the three-phase bridge. I will post the schematic later, thank you。