This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51200: 发热严重?

Part Number: TPS51200


您好,用TPS51200给DDR3提供0.75V VTT和VREF电压,一个板子上面有三个TPS51200,其中两个是4片64位的DDR3,一个是2片32位DDR3,原理图如下: ,严格按照数据手册原理图参考的来的,PCB布局为  ,每个板子的3颗TPS51200布局一样。现在问题是:在红外热成像仪上面观察,有两块PCB的TPS51200在工作中发热严重(红外热成像仪上面显示是80°左右),而这两个TPS51200在一个PCB上是同一个位置,DDR3工作正常。想请问一下这个发热可能原因出在哪里?其中一个更换了一个TPS51200还是一样发热,有没有可能是外围电阻电容器件损坏呢(这个板子裸露测试了很久),或者其他原因呢,谢谢指导!