您好:
新项目对电源需求如下,请帮忙推荐一款合适的电源解决方案,多谢。
Vin: 输入使用1~24V可调电源供电,故VIIN输入为正电源即可;
Vou: -1.5V;
Iout: 平均电流≥10A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
选用降压芯片来做,如果输入电压最大到24V, 选用的芯片大于25.5V.
电流能力建议大于15A,甚至更大。(这个取决于你的电压输入,建议你输入电压大于5V以上)
Hi
我是指参考其负压设计的方式,也就是说降压芯片都可以这样设计成负压输出。
TPS5430是不适合你的设计需求,如上选用降压芯片来做,输入大于25.5V。 电流能力建议大于15A,甚至更大。