This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76942: 应用问题

Part Number: BQ76942
Other Parts Discussed in Thread: BQSTUDIO

 Hi,

1.对于BQ7694202这款AFE,它与MCU之间进行IIC通信时,使用硬件IIC和软件IIC在数据采集和指令的发送方面有差异吗?目前用软件IIC采集电压时电压采集数据会有较大的跳变。

2.目前相同的测试板用的BQ76942来控制CHGDSG进行充放电,使用相同的代码烧录,有的板子可以控制CHGDSG,有的板子上无论给AFE发什么指令都无法导通CHGDSG。经检查AFE可以用BQstudio发送指令导通,想问一下是打开FET还有什么特别的指令需要去配置?

3.在采集电压的时候,一次性采集全部电池的电压和用轮询的方式一次采一个电压再去做其他任务,这两种方式对于数据的准确性有影响吗?

4.温度和电池电压采集使用同样的底层驱动(软件IIC)进行读取,为什么读5个温度的任务的时间比读7个电池电压的时间多十几毫秒?

谢谢!