This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
求一个5V输入,能恒定输出60W的电路,元器件高度小于2.6mm。 感谢推荐。
找个限压限流的线路就可以,TI很多低压芯片,不知你的是升压还是隔压,或升隔压?
建议用LM5122
输出电压、输出电流没有要求?
输出电压在30V以上。感谢推荐。
请问输出恒功率是怎样实现的?是通过控制IC那个PIN脚来实现?是limt来达到的吗?