This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想选一款芯片,可以有多片,输入DC48V,输出:DC 24V@15A,或DC12V@3A或DC5V@3A 最好是同一款或引脚兼容。请推荐,非常感谢!联系方式:changyuezh@sina.com
Hi
不建议采用同一个芯片来做,原因是输出24V/15A是360W,绝大部分的DC/DC芯片不容易做到,或需要额外增加驱动,或者可以用半桥全桥来做。后另外的两路功率比较小,很多DC/DC的芯片都很容易的可以做到。
如果是选择隔离,或者您可以选择TI的UCC28950, 做三路输出。