This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570: BQ25570

Part Number: BQ25570


BQ25570采集能量给超级电容器充电,超级电容器电压升到1.36V后就升不上去了是什么原因呢?

具体描述:使用线性电源作为输入给BQ25570充电,设置充电电压为0.7V,充电电流最大限制为100mA,实际充电电压为0.7V,充电电流为4mA。充电几个小时后超级电容器电压上升到1.36V,之后线性电源电流开始从4mA跳到0mA,一直这样跳动,应该是充不进去电了,超级电容器电压一直维持在1.36V。这是什么原因呢?

如果升高线性电源充电电压到2-5V,是能够给超级电容器冲进电去的。

BQ25570给超级电容器充电0-1.36V充电很慢,这段充电的原理是什么呢?

恳切希望大佬解惑!!!

鞠躬,致谢