When using the LMR14010A chip to output 5V, the output is fully loaded with electronic load 1A, and the power-up waveform of the output will have a hookback greater than 1V. Neither I increased the capacitance value, used the manual reference design, or simulated it with Tina software, I could not eliminate this backlash.
Is this question related to the chip itself? How should it be solved?


,我调试之后最好只能把回勾的幅值减小到200mv左右,但是无法消除