Hi TI expert,
FM天线诊断电路上用的TI的tps7b7701芯片,现在遇到一个问题,天线输出short-to-battery情况下,ERR pin没有被拉低,读SENSE1 ADC通道值是0,看起来和Datasheet page13上不一致,
天线开路open load时候,ADC读值也是0,和short-to-battery就无法区分了,请看下这个问题,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI expert,
FM天线诊断电路上用的TI的tps7b7701芯片,现在遇到一个问题,天线输出short-to-battery情况下,ERR pin没有被拉低,读SENSE1 ADC通道值是0,看起来和Datasheet page13上不一致,
天线开路open load时候,ADC读值也是0,和short-to-battery就无法区分了,请看下这个问题,谢谢!
HI
确认一下是否如下:
At this moment, if the device detects the short-to-battery fault, the LDO switch is latched off, the ERR pin is asserted low, and the fault-channel SENSE voltage is pulled up internally to a voltage rail between 3.05 V and 3.3 V.
HI
参考datasheet 第12页各类保护下的Vsense, err状态。(Fault Table)
如果芯片能正常输出,只是部分保护动作异常,而芯片本身没有问题的话,有可能是保护操作上的问题。
你可以在美国E2E上问一下保护操作: https://e2e.ti.com/ 主要是我这边没有这个芯片的板子以及设备来验证。美国那边应该有这个芯片产品线上的工程师能帮到你。